Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75C1167: output current of a driver

Guru 29720 points

Part Number: SN75C1167

Hi Team,

Recommended operating condition of driver output current shows the following.



question1)
Is ±20mA defined as per single driver?
I believe it but would like to confirm just in case.

question2)
What is concern if output current of driver (1ch) exceeds ±20mA?
My customer estimates it exceeds ±20mA. It is approximately ±21~22mA.

Best Regards,
Yaita / Japan disty