Part Number: TPS2549-Q1
Other Parts Discussed in Thread: TPS2549, TPS2546
Hi,
My customer is evaluation the TPS2549-Q1 with the EVM.
They tried to connect iPhone6S with the TPS2549EVM and switched off the iPhone6S.
After switching off, the iPhone6S restarted automatically.
What is this cause?
They also confirmed followings;
・The iPhone does restart when the TPS2549 is CDP AUTO SWITCH mode(CTL1,2,3,=HIGH), then VBUS drops and rises up.
・The iPhone does not restart when not connected with the EVM.
・The iPhone does not restart when the TPS2549 is SDP mode(CTL1,2=HIGH CTL3=LOW).
・The iPhone does not restart when the TPS254"6" is CDP AUTO SWITCH mode(CTL1,2,3,=HIGH).
Best Regards,
Kuramochi