Part Number: DP83867IR
Hi Expert,
We are using 2 DP83867 on the board and doing connection test, there is an issue that is confusing.
Test set up:
PCB1: 2 PHYs with DP83867, port 1A and 1B.
PCB2: 2 PHYs with DP83867, port 2A and 2B.
Results:
Port 1A connected Port 1B, LED0 Off, LED1 Off, no connection, 2 ports on the same PCB cannot establish connection to each other after power up.
After Port 1x connected to 2x, once the port on PCB1 is connected to PCB2 successfully, the ports on the same board can establish the link to each other without any issue(Port 1A connected Port 1B LED0 On, LED1 On, Ping Good)
PHY on PCB1 always establish successful link with PCB2.
Port 1A connected Port 2A, LED0 On, LED1 On, Ping Good.
Port 1A connected Port 2B, LED0 On, LED1 On, Ping Good.
Port 1B connected Port 2A, LED0 On, LED1 On, Ping Good.
Port 1B connected Port 2B, LED0 On, LED1 On, Ping Good.
Is there any notification for the different PHY with the same DSP/FPGA that may cause this problem?
Thanks.
Zhou
Zhou