Part Number: SN751178
Dear Sirs,
My customer asked us about VOH/VOL of SN751178.
At the output of the Receiver circuit,
What is the certified value of Voh / Vol at current (3 mA, 5 mA, 10 mA, 16 mA, 20 mA)?
(Because、when they use this device, there is a possibility that the current may flow by 5 to 20 mA.)
Best Regards,
Y.Hasebe