Part Number: DP83849IF
Other Parts Discussed in Thread: TS3L501E
Hi
We have designed a board to use DP83849IF as a media converter. the configuration of our circuit is shown in the attached picture.
Our Device Under Test (DUT) has a built-in PHY and MAC chip which normally works with ethernet connection. We have added the DP83849IF to have the fiber functionality. Now the problem is that when I plug the ethernet cable the Link_LED is turned ON for 2 seconds and the activity LED blinks a few time but after that all the LEDs are turned off and DUT does not work.
Have you any idea what might be the problem? could it be a loading/driving issue? I mean because the ethernet port has to drive two magnetics at the same time the link is lost. or is it possible if the data between ethernet port and DUT interfere with the data from media converter.
I haven't tested the fiber functionality yet (input from SFP). but as in fiber configuration the path is only feedforward (ethernet port is NC) is it possible that we will have problems in that case too?
Another point worth mentioning is that in case of connecting the ethernet port the conversion to fiber is not important for us. what is important in both cases is a working DUT.