Other Parts Discussed in Thread: P82B96, P82B715
Hello,
We need a I2C Extender with below specifications:
1) Operating Voltage - 2.5 V to upto 6 V
2) Transmission distance upto 50 meter.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Kiran,
We have the P82B96 or the P82B715 that might be options. Do you have any additional information about the application? 50 meters is a LONG distance. Do we have information about cable capacitance, inductance, and resistance? Also, do you have any information about the data rates they are trying to achieve. This could be a difficult talk to perform. I2C is usually not used in this long of distances.
-Francis Houde