This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65986: TPS65986: Exception in TPS6598x Application Customizer 2_12

Part Number: TPS65986
Other Parts Discussed in Thread: HD3SS460

My Customer is using the Application Customizer to change DP settings on TPS65986.  

To create a new project, we tried to import TPS65986_HD3SS460_UFP_Full_2_10.tpl.

But this is generating an exception as shown in the attachment.

It looks like all the TPS65986 projects generate this Exception.

We also tried with a 82 project, that got loaded cleanly and we could also import the settings from the device.

Are there any known issues or suggestions you might have.