Part Number: LMH0318
Good morning
I want to read the CDR status 1 of the LMH0318 reclocker, In the programming guide I found the register CDR_Status_1 in the Reg_0x02 Channel, the it puts that the bits 3 and 4 indicates the status of the CDR but in the point 4.2.9 Lock Data Rate Indication of the same guide says that only the bit 4 indicates if the CDR is locked or not and furthermore use the mask 0x18, when the bit 5 is reserved.
Someone can indicate me which is the correct sequence to read the status of the CDR?
Thank you