Part Number: DP83822IF
Query is regarding using LINK LED indication from DP83822IF PHY.
As per the datasheet, 4 pins can be configured to use for the LED indication purpose which are provided below (from the page 48),
In page 5, it is provided that LED_0 default function is “LINK indication”
And the register default configuration in page 66 is bit confusing. It says it is routed to COL.
Which pin should be used for LINK indication by default without configuring register?