Part Number: SN65DSI85-Q1
Other Parts Discussed in Thread: DS90UB928Q
My customer is using this device to go from an SoC (DSI) to our DS90UB947 (LVDS) serializer and eventually deserialized by the DS90UB928Q. We are having some issues bringing up the bridge and getting the DSI/LVDS bridge to lock onto the DSI CLK. I’ve run through the register settings several times and I am convinced that they are correct. For the power-on sequence in the datasheet, we don’t know how to bring the DSI CLK and Data pins to the LP-11 state, so this may be the source of the issue. Any help would be great!
I plan to connect a Ref clock today and try to generate a pattern.
I've attached the register settings.
Thanks for your help!
-Joe
//===================================================================== // Filename : DSI_LVDS_Bridge_Settings.txt // // (C) Copyright 2013 by Texas Instruments Incorporated. // All rights reserved. // //===================================================================== i2cset -y 1 0x2d 0x09 0x00 i2cset -y 1 0x2d 0x0A 0x05 i2cset -y 1 0x2d 0x0B 0x10 i2cset -y 1 0x2d 0x0D 0x00 i2cset -y 1 0x2d 0x10 0x26 i2cset -y 1 0x2d 0x11 0x00 i2cset -y 1 0x2d 0x12 0x2c i2cset -y 1 0x2d 0x13 0x00 i2cset -y 1 0x2d 0x18 0x78 i2cset -y 1 0x2d 0x19 0x00 i2cset -y 1 0x2d 0x1A 0x03 i2cset -y 1 0x2d 0x1B 0x00 i2cset -y 1 0x2d 0x20 0x00 i2cset -y 1 0x2d 0x21 0x05 i2cset -y 1 0x2d 0x22 0x00 i2cset -y 1 0x2d 0x23 0x00 i2cset -y 1 0x2d 0x24 0x00 i2cset -y 1 0x2d 0x25 0x00 i2cset -y 1 0x2d 0x26 0x00 i2cset -y 1 0x2d 0x27 0x00 i2cset -y 1 0x2d 0x28 0x21 i2cset -y 1 0x2d 0x29 0x00 i2cset -y 1 0x2d 0x2A 0x00 i2cset -y 1 0x2d 0x2B 0x00 i2cset -y 1 0x2d 0x2C 0x20 i2cset -y 1 0x2d 0x2D 0x00 i2cset -y 1 0x2d 0x2E 0x00 i2cset -y 1 0x2d 0x2F 0x00 i2cset -y 1 0x2d 0x30 0x06 i2cset -y 1 0x2d 0x31 0x00 i2cset -y 1 0x2d 0x32 0x00 i2cset -y 1 0x2d 0x33 0x00 i2cset -y 1 0x2d 0x34 0x50 i2cset -y 1 0x2d 0x35 0x00 i2cset -y 1 0x2d 0x36 0x00 i2cset -y 1 0x2d 0x37 0x00 i2cset -y 1 0x2d 0x38 0x00 i2cset -y 1 0x2d 0x39 0x00 i2cset -y 1 0x2d 0x3A 0x00 i2cset -y 1 0x2d 0x3B 0x00 i2cset -y 1 0x2d 0x3C 0x00 i2cset -y 1 0x2d 0x3D 0x00 i2cset -y 1 0x2d 0x3E 0x00 The PLL_EN bit and SOFT_RESET bit are not set as they need to be set per the recommended sequence defined in the datasheet