Other Parts Discussed in Thread: DS92LV2412, DS92LV2411
Hi all.
I have one question about DS92LV2412.
Please check Table 16 in the datasheet of DS92LV2411/DS92LV2412.
There is discribed the PCB DAP size of DS92LV2412 is 7.2 *7.2 mm in Table 16.
However DS92LV2412 PCB size is 6.3*6.3 mm in P.53.
Is 7.2mm Typo? Which size is correct?
I think the following size is corrct.
2411=5.1mm
2412=6.3mm
Is my understanding correct?
Best Regards,
Sho