Other Parts Discussed in Thread: DS80PCI102
Before I start the question, someone at TI should fix the forum setup. Every time DS80PCI102 is entered in the "Part Number" field "Consumer & Computing Forum" is automatically selected with no other options. I have to pretend not having a part number to start this.
Anyway here are my questions:
1. When the part is powered with ENSMB high and PRSNT# high, is the device accessible from I2C bus? If not, when is the I2C accessible from falling edge of PRSNT#? I understand there's a 500mS restriction from power up.
2. Similar to question 1, Page 15 of the datasheet states that "If PRSNT# is asserted while ENSMB is high, the registers retain their current state." Does it mean registers are not accessible when PRSNT# low? All I'm trying to figure out is how to access the registers and how to have the register values take effect.
3. There're two register fields defined as "Override RXDET", reg 0x02, Control_2 bit [7], and reg 0x08, Pin_Override, bit [3]. Please explain how those two bits and PRSNT# interact.
Thanks.. XZ