Part Number: TUSB7340
Team,
My customer has a question regarding the TUSB7340 PCIe to 4 port USB3/2 host controller IC:
Looking at the block diagram provided it appears that this IC is configured as a USB3/USB2 root hub with 4 ports rather than 4 independent USB3/2 controllers. The reason this is important is that the throughput limitations of a single controller with 4 ports severely restricts the possible data throughput for USB2 operation. Specifically I want to know is if I have 4 USB2 devices all trying to operate at high speed (480Mb/s), will the chip support this throughput, or will it throttle it down to 25% of that due to the 4:1 nature of the internal hub?
Thanks
Viktorija