This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVELT22: Request of IBIS Model

Guru 15520 points

Part Number: SN65LVELT22
Other Parts Discussed in Thread: SN65EPT23, SN65EPT22

Hi,

My customer are requesting IBIS model of following devices.
-SN65LVELT22D
-SN65LVELT23D

I searched the TI Web site, but I can't find it.
Is there a way to get the IBIS model of these devices?
Or Should I contact to local TI FAE?

best regards,
g.f.

  • Hi,

    I found following devices.
    -SN65EPT22
    It seem that this device is pin comatible against SN65LVELT22D, and it's same function device.
    Is it pin compatible?

    -SN65EPT23
    It seem that this device is pin comatible against SN65LVELT22D and it's same function device.
    Is it pin compatible?

    The IBIS model are provided for these two devices.
    So, if there are no IBIS model for SN65LVELT22D and SN65LVELT23D,
    should I suggest SN65EPT22 and SN65EPT23 to the customer?

    best regards,
    g.f.
  • Hello g.f.

    The IBIS models for those devices were requested.

    I will come back to you as soon as the models be ready.

    Best Regards,

    Gerardo

  • Hi Gerardo,

    Thank you so much for requesting the IBIS model.

    If you don't mind, could you let us know the schedule
    when we could get the IBIS model.
    Because if it takes a time, maybe we should suggest other same function device
    which IBIS model are already provided to my customer.
    I'm sorry for asking such a question.

    best regard,
    g.f.
  • Hello g,f,

    The estimate schedule for this model is 2/3/2017.

    Regards,

    Gerardo

  • Hi Gerardo,

    Thank you for the reply.
    I understood.
    I think I should ask to my customer whether they can wait.

    best regards,
    g.f.