Part Number: TLK2711A
Other Parts Discussed in Thread: TLK2501, TLK10031, TLK6201EA
Hello Team,
We are aware that TLK2711/TLK2711A is marked as NRND/Lifebuy and should not be considered for new designs.
Customer needs to design a transmitter to connect to the receive side of an existing design with TLK2711. The existing receiver uses one of two inputs and the second one connected to GND through 50 Ohms resistor.
Couple of questions from customer:-
- What is the max distance can be achieved for reliable transmission at 2.0-2.7 Gbps with a single coax and alternatively a couple coax cables with TLK2711?
- What is the device could be used to convert the serial 2.0-2.7 Gbps data from Altera FPGA (serdes) to be compatible to TLK2711 single ended coax input at max distance about 15 meters?
- In addition to the component in a NRND If you have an alternative component that could replace the TLK2711 from one side and can work in collaboration to TLK2711 in the other side .
Best regards,
Mizanur
Central Apps/EMEA