Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65982: DP/DM short to VBUS

Part Number: TPS65982

Hi,

Assume there's an abnormal type-C device now, the USB HS data (DP or DM) is short to VBUS.  When this device is connected to an NB with TPS65982 on it, DP (or DM ) is short to VBUS which is 5V.  Considering these DP/DM signals from type-C connector are connected to TPS65982, what will happen to TPS65982?  With  DP (or DM) are 5V, will TPS65982 HS MUX still operate normally and pass DP/DM signal to USB host controller?

Thanks!

Antony