Part Number: PCA9544A
Hi,
the 400mW total power wc is for my power derating too conservative and I would like to get some typical numbers for the following config:
PCA9544A
TSSOP20 package
VCC = 3.3 V
bus speed = 100kHz
all pull-up resistors are 4k7
slaves on all 4 channels connected, but only one channel enabled simultaneously
is there a tool or an estimator to get a typical power number for this device? Or can you maybe simulate this?
regards, Bertram