This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD6S300: About D1,D2 absolute maximum ratings

Part Number: TPD6S300

Hi,

Absolute D1,D2 maximum rating is 6V.
However,Braak-down voltage is prescribed (7V).
Please tell me the reason.
And Is D1,D2 maximum rating =6V expression mistaken?

TPD6S300.pdf

Best Regards,
Yusuke/Japan Disty