Part Number: TPS65982-EVM
Other Parts Discussed in Thread: TPS65982, HD3SS460
Hello TI,
I am currently using the TPS65982 EVM with the aardvard I2C/SPI programmer.
For software I am using your TPS65982 application tool to generate .pjt and .bin files
To program the evm I am using the Host interface utility tool
I am able to see the EVM over the SPI and I can read registers in the TPS, so I believe the interface is working.
To generate images I am doing the following
-
Using the application customization tool generate a new project file. I use the TPS65982_HD3SS460_DFP_FULL_2_10.tpl as my starting project.
-
I generate both a flash image binary and a low region image bin file.
-
I then use the host interface tool to program the flash with the low image bin file
However I am unsuccessful in programming the associated flash on the evm and I am unsure of what I am doing incorrectly in my procedure.
Or is there something in my image that is not allowing me to program the SPI flash (indirectly through the I2C interface)
I have appended the .pjt and the .bin files. Is there any-way to get some phone support to possibly discuss this issue regarding programming the EVM for a few minutes...this is becoming a critical show stopper for us….
Regards,
Guy