Part Number: TPS65982
Other Parts Discussed in Thread: TPS65981
Hi,
I have question about VDMs and ADCs command.
1. The Input DataX of "Table 4-20. VDMs - PD send VDM" does not define Bit3.
Is this reserved Bit? If so what is bit value as register write?
2. The Output DataX of "Table 4-38. ADCs - Perform ADC Single Channel Read Operation"
What is "ADCMCTemperature"? Is this possible to access by ADCCan bit "00000"?
Regards,
Ogasawara