This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH0303: 3G-SDI solution of cable driver

Guru 19655 points
Part Number: LMH0303


Is there match device of below request spec?

------------------------------------

①Input spec

 ・I/O standard : CML(FPGA SER output)

        Rterm:100Ω

 ・Data rate : 2.97Gbps

 ・# of lane : 4 lane

 ・Encode : 8B10B

②Output spec

 ・I/O standard : CML(FPGA SER output)

        Rterm:100Ω

 ・Emphasis output

③Other

 ・Interface:3G SDI

 ・Cable length:9m

------------------------------------

I searched LMH0303 and the other series device, but I didn't find match device.

Best regards,

Satoshi

  • Hi Satoshi-san,

    Are you looking for an aggregator or "gear-box" device? From your description, I am not sure if you are looking for some type of 4 IN -> 4 OUT solution or if you are looking for a 4 IN -> 1 OUT solution. If you can reference a comparable device by another vendor, we will have a better idea of what you are looking for.

    This will also help us discern what type of product you are searching for. Currently, I am unable to fit your device specifications into the category of either a cable driver or cable equalizer.

    Thanks,

    Michael