Part Number: TPS2544
Hi,
I'm planning to use the TPS2544 as a DCP controller (no CDP). I prefer this chip to other options since it changes between modes automatically, even between Divider1 and Divider2. Since I wont be using pins 2 and 3, respectively DM_OUT and DP_OUT, should I leave them floating (no harm comes from this) or can I connect them to ground for better heat dissipation to the PCB (and added ESD protection)?
My configuration is: CTL1=0; CTL2=0; CTL3=1; ILIM_SEL=1. I have a 22.6K resistor connected to ILIM_HI and no resistor connected to ILIM_LO.
Thanks in advance.
Kind regards, Samuel Lourenço