Do the SN65LVDS1, SN65LVDS2 LVDS devices have requirements on the MAXIMUM input rise (and fall) times?
Some application notes state that long rise/fall times may lead a LVDS device to oscillate on the “slow” input level changing.
What are the absolute maximum input rise/fall times for the SN65LVDS1 IC to work without oscillation on the input signal edges?
Unfortunately but their datasheets contain no such information.
Thank you,
Alexander