This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MAX3243: Could we apply a RS232 level on RINx pin (RS232 line data input) when the IC is not powered (VCC=0).

Part Number: MAX3243


Hello,

In a project i want to use MAX3243 IC.  In particular situation, MAX3243 is not powered, whereas RS232 signals are present (imposed by a RS232 peripheral).

So I have 2 questions:

Could we apply a RS232 level on RINx pin (RS232 line data input) when the IC is not powered (VCC=0).

When Vcc=0V, what is input impedance of RINx pin?

Thanks

Sylvain B