Part Number: TLK2501EVM
Other Parts Discussed in Thread: TLK2501
Hi,
I have two boards TLK2501 EVM that i want connect with optical fiber. In each board I have mounted a clock generator with frequency = 125MHz and i have two power supply VDD =2.5 V e VCC=3.3V,
Connector J7 in each board are in this state:
TESTEN = GND
PRBSEN = GND
LOCKREFN = '1' or "high"
ENABLE = '1' or "high"
TX_ERR = GND
LOOPEN = GND
TX_EN = '1' or "high"
I have mounted in each board the optical transceiver (pn HFBR 5961ALZ).
In this configuration, if i connect the two boards with SMA cable, i see the same signal on the oscilloscope the signals TD0 (Connector J1 of board #1) and RD0 (Connector J3 of board #2).
If i connect the optical interface with loopback with TXP and LTXP etc etc, i see with the oscilloscope the signal RD0 (Connector J3 of board #2), with a lot of noise.
which is the correct configuration to transmit in optical fiber between two evaluation board? some advice?
I have the screenshot of the setup and the wave form if necessary.
Best regards
Marco