Part Number: DS25BR150
Hi
do i need some external pull up/down resistors if i have no driving output connected to the ds25br150 input?
thanks for your answers
br
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS25BR150
Hi
do i need some external pull up/down resistors if i have no driving output connected to the ds25br150 input?
thanks for your answers
br
Hi Robert,
The DS25BR150 does not have an internal mechanism to shut off the output when no signal is present on the input. The LVDS circuitry is relatively high gain so even the 30mV of noise will translate into relatively full swing output oscillations. We recommend using a fail-safe bias in case there is no input provided to the DS25BR150 while the device is on. A fail-safe circuit looks similar to below:
You can also find more information about Fail Safe Biasing in AN-1194: www.ti.com/.../snla051b.pdf
Thanks,
Michael