Part Number: TLK10081
Other Parts Discussed in Thread: TLK10022
I have a customer asking the following questions regarding the TLK10081:
In our case we would be taking 4 x 1.25 Gbps ethernet signals (8B/10B encoded) and transporting them optically, ideally at the rate of 10.3125 Gbps, because that is what it appears many of the SFP+ modules support (10 gigabit ethernet rate). There would be a lot of unused bandwidth which could be used for what the data sheet calls a "reserved lane" (see page 13). In our application, the networks being transported could contain sensitive information and thus we have to demonstrate to our customer that no "cross contamination" between lanes is possible. In other words, we have to be absolutely certain that the signal input onto Lane 1 comes out on Lane 1, (same for lanes 2,3,4,etc.). I am hopeful that the "reserved lane" measures indicated on page 13 of the data sheet would accomplish this. I do understand that the traffic is being aggregated and carried together on the same 10 Gbps stream, however, in our application, the "lane ordering" has to be maintained.
There are a couple of questions that come to mind in this regard:
(1) In the case of link disruption, how quickly would the lane ordering be restored?
(2) In the case above, how much potential data could come out of the wrong lane prior to restoration of lane ordering?
I know it sounds kind of paranoid, but these are the things that our customer and the accreditors will want to know.
I was not sure how to answer this as I am not exactly sure how the data is aggregated in the lanes. Can you look at this question and let me know if the TLK10081 will work for them or if we have another device that will meet their need better.
Please let me know if you have any further questions for the customer.
Thanks for your help with this!
Richard Elmquist