Part Number: DS100KR401
Other Parts Discussed in Thread: SN65LVCP114, , DS125BR820, DS125BR401A, DS125BR401
I have a media converter design that converts between 10G-KR and 10G-SR (copper to fiber).
I was having issues getting the 10G-KR side to link/pass data. I obtained an SN65LVCP114 development board and by adjusting settings I was able to improve the signal enough that the converter now would link and pass data at 10G. This was great! However, I then discovered that the SN65LVCP114 was only rated for -10DegC and my application requires a device that will operate at -40DegC.
I then looked at the DS100KR401 and it looked like it would perform similar signal conditioning functions to the SN65LVCP114 WITH a temperature rating down to -40DegC. This seemed like it should solve my problem. I obtained a development board for the DS100KR401 and hooked it up in place of the SN65LVCP114. I can now get my converter to link at 1G data rate but when I try at 10G, none of the settings are producing results like I had obtained with the SN65LVCP114.
Does anyone have any ideas what might be wrong? Is it in error to conclude that the SN65LVCP114 and the DS100KR401 would provide a similar function from a signal conditioning standpoint? The other thing we were going to try is running the SN65LVCP114 down to -40DegC in a temperature chamber. I know that it is not rated there but is it likely that it would function without problems at -40DegC?
Any help with this would be greatly appreciated.
Thank you,
Mike