This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS10CP152Q-Q1: Does the DS10CP152 support 1.5Gbps per channel?

Part Number: DS10CP152Q-Q1
Other Parts Discussed in Thread: DS10CP152


You need to make sure that DS10CP152q-q1 supports 1.5 Gbps per Chnel.

We tested the 1280 * 720P 30fps image with FPDLINK3 Single Ended in DS10CP152q-q1 and tried to use the output in two places,

but the output at Pclk 84Mhz is half as 47Mhz, H / V Sync output does not work.

Input resolution: 1280 * 720p

Pclk: 84Mhz

Bit: 10bit

Use Serializer: DS90UB913

Use Deserializer: DS90UB914

The hardware configuration is shown below.

Thanks.