Part Number: SN65HVS882
In Figure 21 of the datasheet, an application circuit demonstrating the system protection for the SN65HVS882 device is shown. for the input terminals, it depends barely on the 1.2kW resistor.
My question is:
- what is the maximum protection this circuit offers in case of Continuos voltage (mis-wiring) and Surge event?
- in case of 1kV surge event, we will have ~1A for about 20 uS, where this current will flow after capacitor charging? there is no information in the datasheet about the maximum current in case of ESD event and for how long it can flow. only the normal operation 5mA limit.
- if the device is relying on internal diode to channel this current to the VCC, can this diode withstand such current?
- in case of Continuos voltage of say 30V, there will be 25mA of current through the 1.2kW resistor while normal current limit is 5mA. what is happening in this case? increase of pin voltage and turn on of the ESD structures leading again to a condition like above with less current?
Those questions are related to a Customer opportunity which we are working on right now.
Thanks in advance!