This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB949-Q1: DS90UB949-Q1 can't capture the input HDMI input signals

Part Number: DS90UB949-Q1

Dear Technical Support Team,

     I use DS90UB949-Q1 to serialize a HDMI  signal to FPD LINK III ,and the derserialized point is DS90UB940. I didn't config the register except reset the bit 4 of the address 0x01 register to reset the HDMI controller after my I.MX6 board output the hdmi signal.When I read 0x5f HDMI Frequency register, I got a result 00. I conform the I.MX6 board output the HDMI signal.and the TMDS_CLK 's frequency is about 26MHz to transfer a 800*480 video signal @60 fps.I use a FFC  cable to connect the HDMI signal between the I.MX6 board and 949 board

    Need I config other registers to resolve the problem? What is the mechanism of the input HDMI clock locking of the 949? I measured the single end signal of the HDMI clk,and I got a poor rising edge and falling edge. Would it be the reason that I can't get the frequency of the TMDS_CLK?