Part Number: TPS2511
Hi Team,
I am looking at the TPS2511 datasheet and am seeking clarification on a couple of tables..
Assuming I am supplying 5V to my device for charging..
In the first table, a DCP is specified to provide 1.5A:
5V @ 1.5A = 7.5W
However, there is a 10W setup available:
With 5V at the output, this means I am not charging at 2A..
To achieve this 10W output, does that mean I have to increase my voltage output to >5V since the standard for DCP is 1.5A? I am a little confused on the industry standard for fast charging at 5V. Any clarification would be super.
Thanks in advance.
Jared