Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1310A: Abnormal waveform of PCLK

Part Number: TUSB1310A

Hi,

The abnormal waveform of the PCLK is outputted such as following.

PCLK output.xlsx

Conditions are following;

- The strapping option settings are;

   clock source = clock,  input reference clock frequency = 40MHz

- External oscillator frequency is 40MHz

- The PCLK can change into normal by RESETN

What is the cause of this abnormally waveform and the countermeasure?

Best Regards,

Kuramochi