Part Number: DS90UB947-Q1
Hi E2E,
My system has 2 levels hop. i.e. TX -> RX/TX -> RX/TX (3 units connected).
There are I2C slaves with the same initial ID in each unit and I want to access them from the 1st TX.
-Can I achieve this through the use of registers "SLAVE_ID[7:0] " and SLAVE_ALIAS_ID[7:0]?
(ref: registers 0x07, 0x08, 0x70, 0x71, ..... page 60 in data sheet)
-Should the TX EX devices in repeat mode or not?
Thanks!
Michael