This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8041: TUSB8041 default register settings

Part Number: TUSB8041

Hello team,

I have a customer who is looking for a listing of all of the defaults for all the registers for the TUSB8041. I found a similar post at 

https://e2e.ti.com/support/interface/digital_interface/f/130/t/407232 but it was resolved internally. Is there a document I could forward the customer ?

Thank you for your time.

Kishen

  • Hello Team,

    Could you point me towards getting this information for the customer.

    Thank you,

    Kishen
  • Hello,

    The default values are specified in the datasheet as the "Reset state" in every Register.

    I am attaching a .txt file with the EVM's configuration.

    This .txt file can be used along with the EEPROM Programmer tool to program the EEPROM via USB.

    If you require that tool please contact joel.jimenez@ti.com

    Regards

    00	55	01010101	'ROM Signature - Do NOT modify!
    01	51	01010001	'Vendor ID LSB - Can be modified
    02	04	00000100	'Vendor ID MSB - Can be modified
    03	40	01000000	'Product ID LSB - Can be modified
    04	81	10000001	'Product ID MSB - Can be modified
    05	10	00010000	'Device Configuration - U1U2 ON
    06	00	00000000	'Battery Charging (1 = enabled) - Can be modified 
    07	0F	00001111	'Device Removable- Can be modified 
    08	0F	00001111	'Port Used - Can be modified
    09	00	00000000	'Phy Custom - Can be modified
    0A	22	00100010	'Device Configuration 2 - Can be modified
    0B	00	00000000	'usb 20 Port Polarity
    20	09	00001001	'Language ID - Can be modified
    21	04	00000100	'Language ID -  Can be modified
    22	00	00000000	'Serial Number String Length -  Can be modified
    23	00	00000000	'Manufacturer String Length 
    24	00	00000000	'Product String Length 
    F0	00	00000000	'Additional Features
    
    
    
    'DATA FILE FORMAT: <HEX ADDRESS><TAB><HEX DATA>. EVERYTHING AFTER <DATA> IS IGNORED.
    'USE <'> FOR IN-LINE COMMENTING.
    'DATA FILE PARSING STOPS AT FIRST BLANK LINE.