Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPL7407L: TPL7407L without Power Supply

Part Number: TPL7407L
Other Parts Discussed in Thread: ULN2003V12

I want to use a TPL7407L as a replacement for ULN2003. Unfortunatelly, the COM-Pin (Pin 9) is not connected in my circuit, as it was not necessary for ULN2003. The IC drives only LED's with a current of 2mA. I tried the TPL7407L in the circuit - and it works without a power supply on the COM-Pin. Do you think, using the TPL7407L without power supply can cause a problem (Pin open....)?

Thanks in advance,

best regards

Norbert