Part Number: P82B96
Hello Sir/Madam,
We are using P82B96 I2C Extender on our system to connect a sensor to controller which is placed at 6 meters away.
Below are my specs:
Voltage at Sx/Sy side- 3.3V
Voltage at Tx/Rx side 5V
I need to connect two devices which shall run at 400KHz and 800KHz respectively. Could you please help in calculating Pull up resistor values for the same.