Part Number: DP83867IS
Hello. I have a design challenge that I want an advice for. On a VPX system I need to convert the two 1000BaseBX Ethernet interfaces (both according to VITA 46.9) into RJ-45 / 1000BaseT. I was thinking simply to use an DP83867ISRGZT for this. Now the question is : will DP83867ISRGZT SGMII interface connect directly to 1000BaseBX signals in the backplane ? any additional advices on this ? I can add a small MCU to set up the DP83867IS if necessary.
Any help or comments appreciated.
BR Erik