This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPL0102-100: Is there any roadmap for designing quad channel of TPL0102-100?

Guru 29720 points
Part Number: TPL0102-100

Hi Team,

Is there any roadmap for designing quad channel of TPL0102-100?
My customer wants the device that has end-to-end resistance of 10kΩ (x 4) with same package size of TPL0102-100.

Best Regards,
Yaita / Japan disty

  • Yaita-san,


    I've moved this post to the I2C Forum. I believe that all of the digital potentiometers have been supported through this forum (even ones that do not use I2C communications).


    Joseph Wu
  • Hello Yaita-san,
    There currently isn't one on the road map but if you want, please send me additional information about the business case for the device and I can forward it to the systems engineers and see if it might be a good candidate for a future product.
    -Francis Houde
  • Hi Francis-san,

    Thank you for your kind support.
    I would like to replace AD5144 (quad channel) but I understood there isn' t on roadmap.
    My customer's application requires small package size (board space is restricted). 

    Please let me contact again if I need your additional support.

    Best Regards,
    Yaita