Part Number: TPS2549-Q1
Hello Team,
The customer do not like UVLO fuction of TPS2549-Q1, so they are considering the following figure..
1) Is it possible to use TPS2549-Q1 as the folowing diagram?
2) Is the load register and load capasitor required at OUT(12pin) if the answer of question 1) is yes?
3) What value of load capasitor is required? The customer would like to use smaller capasitor than 22uF.
Would you please advise ?
Your help would be so appreciated.
Best Regards,
Akihisa Tamazaki