I would like to confirm the below two points.
1. The back channel frequency is 5.5MHz. Is it correct?
2. Are there any sources of around 30MHz inside of IC?
The conditon is 10 bit mode and pclk = 100MHz.
Best regards,
Atsushi Yamauchi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I would like to confirm the below two points.
1. The back channel frequency is 5.5MHz. Is it correct?
2. Are there any sources of around 30MHz inside of IC?
The conditon is 10 bit mode and pclk = 100MHz.
Best regards,
Atsushi Yamauchi
Hello,
Back channel frequency is 3.3MHz min. to 4.2MHz max. It can be found in the 914A datasheet.
I assume "sources in side of IC" is the internal PCLK frequency. It's 50MHz.
Best Regards,
Sugiura