This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDS179: unused pin

Guru 29720 points

Part Number: SN65LVDS179

Hi Team,

How to do with unused input and output if unused?
I would like to know the following two patterns.

- if driver is unused
LVTTL input signal (3 pin): gnd?
Differential non-inverting output (5 pin): open?
Differential inverting output (6 pin): open?

- if receiver is unused
LVTTL output signal (2 pin): open?
Differential non-inverting input (8 pin): gnd?
Differential LVDS inverting input (7 pin): gnd?

Best Regards,
Yaita