Part Number: TCA6416
Tool/software: Starterware
I am trying to appeal to TCA6416, but the problem is that it does not respond to ASK.
I check the whole l2c bus in cycle and TCA6416 is the only thing that is not seen there.
I also have TCA6416 and i have the same problem with it.
Here's a sample code:
uint8 i2cWriteBuffer[2] = {0x06, 0x00};
I2C_Transmit(0x20 << 1, (uint8*)i2cWriteBuffer, 2);