Part Number: TPS65982
I am connecting to a laptop with the Intel VID Config register setup for TBlt.
In order for it to go into Tbolt Mode (confirming with the status register) I need to use an EMarked cable that has a SOP' message.
If I use a non marked cable the TPS65982 won't go into Tbolt mode.
I tried setting the bit in the config register (0x52) called "TBT Emarker Cable Override" using an Aardvark and writing to the register. (SEE BELOW)
I then disconnect and reconnect the unmarked cable. The PD contract is made, but it won't go into TBolt mode. How does this bit work?