This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ESD PROTECTION REPLACEMENT

Guru 13485 points

Other Parts Discussed in Thread: TPD2E2U06

Looking for recommended replacement to NXP P/N VBUS54CV-HSF?

The TPDxE05U06 as lower performances as has only 

±12-kV Contact Discharge

– ±15-kV Air Gap Discharge

NXP device has 

± 30 kV contact discharge

± 30 kV air discharge

  • Hi Eli,

    I would be glad to help you choose the appropriate part for your system. First, can I get some of the system specs from you? Do you need ESD protection up to 30kV?

    Very Respectfully,

    Brian Dempsey

  • High ESD is important as it for medical application.

    Looking for TI best replacement if we have

  • Eli,


    The TPDxE05U06 is probably the best selection with respect to competing with the line capacitance and leakage current of the vbus54cvhsf. Unfortunately, as you have stated, the device is rated for 12/15 kV.

    Alternatively, the TPD2E2U06 could be used for higher IEC ratings, rated for 25/30 kV. This is a 2-channel device though, so there would need to be additional real-estate available on the board for a second ESD chip. Our line capacitance is 0.3 pF larger than that of the vbus54cvhsf, but this should still be suitable for the application. Hope this helps!


    Very Respectfully,

    Brian Dempsey