Part Number: DP83867IR
Hi
I'd like to know the configuration of Mirror mode.
I know that Mirror mode can be enabled/disabled via strap or register configuration.
But it seems that "After Mirror mode is enabled once, it can't work properly if Mirror mode is disabled after that".
The port connections of my customer board is not mirroring. So, they usually use it with Mirror mode disabled.
But, at first, Mirror mode is enabled via strap. And then, they changed Mirror Mode register configuration using MDIO. As a result, it doesn't work.
====================
1. Mirror mode is enabled via "strap",
2. Mirror mode is disabled via "register configuration" using MDIO.
=>NG: Link is established. But there is no data on RGMII RX signals if there are some "Receive activity". (LED2 is lighting)
====================
1. Mirror mode is disabled via "strap",
=>OK! no problem.
I checked it using EVM. I confirmed the same phenomenon happens.
So, I understand that "After Mirror mode is enabled once, it can't work properly if Mirror mode is disabled".
Is my understanding correct? Or we need to config any other register when Mirror mode is changed?
Of course, I think Mirror mode should be disabled via strap for this board.
Best Regards,
Taka