Part Number: DP83959
Hi.
I want to use DP83959 to deliver and restore a pure clock signal to the other board through an ethernet line.
Fundamentally, the purpose of my project is estimating location of USER, and I'll use AP boards.
For this, I have to synchronize CLOCK signal of all AP boards.
And for synchronization of CLK, I'll use EHTERNET LINE.
But, basically, I have to place the anchor AP boards with 100m distance between each boards. And unfortunately, In environment of my experimental space, usable CLK signal is maintained to 50m.
So I have to extend it. And I want to use DP83959 for it.
Is it right application? Can I use DP83959 for deliver the restored CLK without delay or minimum fixed delay time?
Unless I can not use it, could you please recommend other chipset or product?