A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I could check the HVD10 circuitry; for the other devices, it would be best to post in the respective forums for each device in order to get the right people to review it. For the HVD10, though, it looks like the DE pin is tied high, meaning the device is always used as a transmitter. Is this your intention? This would make it impossible for other nodes to transmit on the same bus, so this could only be used for "broadcast" (one transmitter / one or more receiver) applications. You should also make sure that a decoupling capacitor is used on the VCC rail; 0.1 uF would be a good value. You should also make sure to terminate the RS-485 signal using a resistor between the "A" and "B" line that matches the characteristic impedance of the cabling you plan to use (120 Ohms is common).