This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65982: TPS65982 read image issue in application customization tool

Part Number: TPS65982


Hi Team,

Customer is using TPS65982 application customization tool. He can’t see the register setting read from the working sample.

The previous image is generated by using the TI web tool,  it is now change to the TPS65982 application customization tool, so he wants to read out the original setting and modify for his new application. Do you know how to do this?

Thanks.

Regards,

Tony Wen

  • Hi Tony,

    When connecting the device to your computer through either the FTDI or Aardvark, you can import the settings from the attached device into the Applications Customization Tool. To do so, first attach the device, then in the Application Customization Tool click Device -> Import Settings From Device. This will import the current config into the tool. You can then make edits to the configuration and create a new binary Flash Image to load onto the device.
    To load the new flash onto the device, use the Host Interface Tool and click on SPI FW update.

    Thank you,
    Eric