We have a need to programmatically mock HPD as well as a Display Data Interface which provides and EDID to a host PC.
1) Is there any reason we shouldn't be able to 'fake' the HPD dialog over the CC line by sending "Attention" packets? Confirmation of success would be the display "blink".
2) Once the HPD is received, is it reasonable to expect the host PC to poll the SBU lines for an unadulterated (beyond polarity) DDI signal? Meaning, in the simplest sense of a VGA/HDMI display, will the PC GPU then be expecting an I2C slave on SBU1/2 ready to provide an EDID?
Thanks all!